Motor control - igus Blog - Page 5 Motor control - igus Blog - Page 5

Tag: Motor control

Which DC motors can be connected to the D3 DC motor control?

Michael Hornung | 8. July 2019

See here the types of DC motors that can be connected to the D3 motor control. A tip: It’s easy to order DC motors (and also stepper motors) in the online shop for electric motors, available from stock with no minimum order quantity. Tip For those of you who want to know and read more […]

Read more...

How are the digital outputs of the d1 motor control connected?

Michael Hornung | 8. July 2019

Easy to understand in practical steps, demonstrated by the following video. If you want to know more about commissioning the dryve D1 motor control, you can find the complete manual here. Vote Up +0 Vote Down -0You already voted!

Read more...

How do I connect a proximity switch to a D3 DC motor control?

Michael Hornung | 8. July 2019

The proximity switches, which are inductive as limit switches, offer greater process reliability when operating a linear axis.  Waterproof, dustproof and no mechanical or electronic wear. These are the advantages over using mechanical proximity switches. You can see here how to connect the inductive proximity switch to the D3 DC motor control.   Tip For […]

Read more...

CanOpen and the fast connection to the D1 motor control

Michael Hornung | 8. July 2019

In a few seconds, the D-Sub connector for the CAnOpen connection is mounted to the dryve D1 motor control. Here is the video shown in a few seconds. Tip For those of you who want to know and read more about the operation of the D1 dryve motor control, see the complete manual here. Vote […]

Read more...

Is it possible to integrate the D1 into a higher-level control system?

Michael Hornung | 1. July 2019

Yes, that’s possible. The available communication interfaces make connecting to a higher-level industrial control system such as a PLC or an industrial PC very easy. But not only that … the D1 works just as well with microcontrollers like an Arduino or single-board computers like the Raspberry Pi. Thus, the D1 is also well prepared […]

Read more...