Outdoor use is generally uncritical for energy supply systems. Energy chains are very tough and withstand extreme temperatures below freezing. Each energy chain is tested in the igus in-house test laboratory in a refrigerated container at -40 degrees Celsius and on an outdoor test track under real conditions. For special requirements, energy chains are also […]
The service life of the rollers of an energy supply system generally depends on the roller material and the external environment. Free-running or unprotected rollers are exposed to external influences. In energy chain systems, rollers are integrated in the chain link and “lubricated for life” with a seawater-resistant lubricant. A replacement for such a system […]
There is a bearing point for pivoting movement in every connection of the chain links. This was equipped with a maintenance-free tribo-polymer plain bearing. The igus iglidur plain bearing ensures that the wear on these “joints” of the energy chain is kept to a minimum and that the service life can be significantly increased. In […]