The chain length calculation (only in German) is made for an unsupported or gliding application. Unsupported: If the supply point is outside the centre, the formula for calculating the chain length is as follows: K = π x R + (2 x T) Lk = length of the e-chain S = length of travel S/2 […]
Energy chain systems not only transport energy, data and media to machinery and equipment. They also have an influence on their energy costs. How much pull and push force, in other words drive power, is required at a given speed to move an energy chain? How light but at the same time sturdy must energy […]
What is decisive often is not the pros and cons of the individual systems but if the particular system is the right energy supply for my application in terms of cost, durability and installation space. For example, if you compare only motorised cable drums to energy chains, there is no blanket answer, because in the […]
Outdoor use is generally uncritical for energy supply systems. Energy chains are very tough and withstand extreme temperatures below freezing. Each energy chain is tested in the igus in-house test laboratory in a refrigerated container at -40 degrees Celsius and on an outdoor test track under real conditions. For special requirements, energy chains are also […]
The service life of the rollers of an energy supply system generally depends on the roller material and the external environment. Free-running or unprotected rollers are exposed to external influences. In energy chain systems, rollers are integrated in the chain link and “lubricated for life” with a seawater-resistant lubricant. A replacement for such a system […]