Load - igus Blog Load - igus Blog

Tag: Load

What do I do if the unsupported length is exceeded?

Marco Thull | 3. July 2019

If the unsupported length of a series is exceeded according to the FLG diagram (fill weight, travel), the following options are available. Choose a more stable e-chain. Example: E4.42, additional weight 15 kg/m; travel/unsupported length: 5 m/2.5 m Under these conditions, the E4.42 is in “critical sag”. If an energy chain is required in the […]

Read more...