Filament - igus Blog Filament - igus Blog

Tag: Filament

How accurately can a 3D printer print?

Dirk Zacharias | 1. August 2019

The accuracy of a 3D printing part depends on the respective method and the quality of the printer. The filament used and the quality of the CAD data also play a role here. Basic information on tolerances in 3D printing Compared to injection moulding or machining processes, the possible deviations are greater in 3D printing. […]

Read more...

When is direct 3D printing more suitable than print2mold?

Dirk Zacharias | 1. August 2019

For example, if the delivery must be extremely fast – 24h up to a maximum of 3 days. In addition, the more complex the component, the more beneficial it is to make the components directly in 3D printing. Due to the tool-less manufacturing, complexity does not cause any additional costs. For small parts under 5 […]

Read more...

What is the FDM method?

Dirk Zacharias | 30. June 2019

Fused Deposition Modeling (FDM) is a 3D printing method whereby a material such as plastic is melted to create a 3D object layer by layer. Fused Deposition Modeling is an additive manufacturing method and is also referred to as the fused layer modeling method. The plastic or metal material that is processed is called filament. […]

Read more...