Energy chains - igus Blog Energy chains - igus Blog

Tag: Energy chains

Where are smart plastics used in the port?

Richard Habering | 22. September 2021

Heavy loads, long periods of use, and a wide variety of weather­­conditions – cranes in port facilities must perform at their best. The fields of application include, among others, ship-to-shore cranes, bulk cargo handling cranes, RTGs, RMGs, Goliath cranes, spreaders and reach stackers. In total, more than 25,000 igus energy chains move across long distances […]

Read more...

What is so special about smart, or intelligent, rol e-chain® for cranes?

Richard Habering | 22. September 2021

To load and unload the cutting-edge – keyword Triple E-class – container ships, larger STS cranes must be built or existing cranes retrofitted. Container crane availability and dependability requirements are also increasing. For future operations, in addition to using rol e-chains, there is much to recommend self-monitoring systems fitted with sensors . They ensure the greatest possible […]

Read more...

How is condition monitoring of the energy supply on container cranes implemented?

Richard Habering | 22. September 2021

More than 25,000 igus energy chains move over long distances every year, whether in STS cranes, storage and retrieval units or linear robots. In all these areas of application, customers around the world rely on the tough, modular igus energy chain systems. In the latest development stage, maintenance-free tribo-polymer plain bearings considerably lengthen service life. In […]

Read more...

Are there any energy supply system for cleanroom class 1 and 2?

Phillip Hagedorn | 6. July 2019

Yes, igus offers different e-chains, which can also be used in a cleanroom. Extensive tests were carried out with the energy chains for this purpose at the Fraunhofer Institute. A selection of qualified e-chains can be found here. ISO Class 1: E3, E6.1, E6, e-skin ISO Class 2: easychain, zipper, E2 mini*, E2.1*, E2/000 E4.1*, […]

Read more...

What does ISO Class mean?

Phillip Hagedorn | 6. July 2019

All products used in cleanrooms need to fulfil the same requirement: During operation, as few particles as possible should be released into the surrounding area. This is especially applicable for moving machine parts such as energy chains and cables. To generate as few particles as possible requires high abrasion resistance, and is therefore also an […]

Read more...