cables - igus Blog - Page 3 cables - igus Blog - Page 3

Tag: cables

What is electrical resistance soldering?

Beke Nieszytka | 25. September 2020

During the process of electrical resistance soldering, the parts to be joined are pressed together with tongs or welding heads, and by supplying electricity, the solder is melted electrically at the contact points between the components.

Read more...

PoE – power via a network cable

Julian Dymek | 13. January 2020

Power Over Ethernet (PoE) is a function that makes it possible to transmit electrical power as well as data via an Ethernet cable. The advantages are considerable as an additional cable for power supply is not necessary. Devices such as WiFi access points and IP web cams can therefore be connected to the infrastructure and […]

Read more...

Is there anything to monitor the condition of cables?

igu-blog-adm | 9. July 2019

With CF.Q, CF.D and CF.P, igus has three sensors in the product range that are designed for chainflex cables. CF.Q is the sensor for the electrical specifications of chainflex cables Belongs to prevention of crash and can be used without an additional module Indicates changes in the electrical properties In the event of a fault, […]

Read more...

What are the connection types available?

Beke Nieszytka | 8. July 2019

The following connection types are available: Screw connection Axial screw connection Crimp connection Cage clamp connection Solder connection Wrap post connection Insulation displacement connection Press-fit technology Fibre optic connection Vote Up +1 Vote Down -0You already voted!

Read more...

Can harnessed cables also be individually labelled?

Beke Nieszytka | 8. July 2019

Yes, harnessed cables can be customised.All harnessed cables are marked with a label on each side. In addition, many cable inscriptions can be stamped, embossed, engraved, lasered or printed with industrial grade ink. Vote Up +1 Vote Down -0You already voted!

Read more...