Bearing change - igus Blog Bearing change - igus Blog

Tag: Bearing change

Bearing change on the rail in 30 seconds

Michael Hornung | 30. June 2019

An outstanding component of the modular drylin W linear system is the WJ200UMA exchange bearing. With this type of linear bearing, the liner can be changed directly on the rail. No linear housing, no linear carriage, no linear module, no delta robot needs to be removed for this. All four bearings can be replaced in […]

Read more...

How are bearings changed in the case of a low-profile guide system?

Michael Hornung | 30. June 2019

The drylin N low-profile guide system consists of an anodised C-profile in which a sliding carriage travels. The basic carriage is a zinc die-cast component and is clipped into a sliding frame made of iglidur J polymer. Completely dry, clean and quiet when sliding. The two halves of the sliding frame can be ordered at […]

Read more...