To load and unload the cutting-edge – keyword Triple E-class – container ships, larger STS cranes must be built or existing cranes retrofitted. Container crane availability and dependability requirements are also increasing. For future operations, in addition to using rol e-chains, there is much to recommend self-monitoring systems fitted with sensors . They ensure the greatest possible […]
More than 25,000 igus energy chains move over long distances every year, whether in STS cranes, storage and retrieval units or linear robots. In all these areas of application, customers around the world rely on the tough, modular igus energy chain systems. In the latest development stage, maintenance-free tribo-polymer plain bearings considerably lengthen service life. In […]
According to research performed by Accenture Technology, a globally active consultancy, the successful implementation of predictive maintenance can have a marked impact on the performance of industrial organisations across sectors, saving up to 12% over scheduled repairs, reducing overall maintenance costs by up to 30% and increasing breakdown avoidance by up to 70%. Accenture cites […]
In its first stages, IIoT was limited to high-value, big-ticket technologies such as aircraft turbines, for which the enormous costs associated with failure justified the investment. But now there is a discernible trend towards communication-capable, intelligent devices being used to create integrated systems at the lowest level of the automation pyramid. The current development is […]
Energy chains are put through their paces at igus’ in-house test laboratory. In linear movements of different lengths with travels of up to 240m and in vertical, circular or torsional movements. 53 test rigs on which 295 tests are simultaneously carried out are used to test e-chains for their stress resistance. In all, 4,100 tests totalling 10 […]