In addition to the tests carried out in the framework of the material quality inspection, iglidur plain bearings are subjected to special wear tests by igus. Every iglidur material is tested for its wear properties in hundreds of stress scenarios, whereby different plain bearings with diverse dimensions are tested. The data are recorded systematically and are the […]
Many manufacturers declare their products to be “maintenance-free”. This usually means that the bearing in question is delivered with initial lubrication. As long as this lubrication is intact, no maintenance of any kind is necessary. iglidur plastics, in contrast, do not have a lubricating film and no reservoir of grease that is eventually used up. The […]
Yes. iglidur PRT-01-20-C and PRT-01-30-C are types that can be clamped on shafts. If required, we also make split PRTs that can be fitted around cable harnesses or tubes. Vote Up +0 Vote Down -0You already voted!
All iglidur materials have advantages in this respect. They are insensitive to dirt, completely corrosion-free and do not need any lubrication. In many places where bearings are used in the agricultural area, large forces as well as impacts and shocks have an effect. Especially robust and durable iglidur materials such as iglidur G or iglidur M250 are particularly suitable […]
Due to the different manufacturing methods, we are able to offer economical solutions for every need: from rapid prototyping to large series from complex injection moulds with multiple activities. And all this without any minimum batch size or minimum order value. Vote Up +0 Vote Down -0You already voted!