In e-ketten, all media can be guided easily and safely – including hydraulic and water hoses. Ideally, they are laid individually and are allowed 20% extra installation space. Their behaviour under pressure is to be considered when a choice is made, also when the strain relief system and interior separation layout are selected. For such […]
After proper installation and correct adjustment of the cables, the dependable system can be started up. Depending on the application and the travel frequency, occasional visual inspections and re-adjustments of the cables are recommended. Otherwise, the energy chain as such is completely maintenance-free. Vote Up +1 Vote Down -0You already voted!
All media can be supplied safely and reliably with only one energy chain system. Vote Up +0 Vote Down -0You already voted!
With the e-spool – the slipring-free cable reel – igus supplies energy supply systems for different scenarios of use. The compact, spring-driven system can guide energy cables, media lines or fibre optic data cables safely and reliably. To enable users to deploy an energy chain system even where greater cable/hose lengths are involved, igus has […]
An additional drive is not needed for igus e-chain systems. As a result, the number of necessary components is reduced, and commissioning is simplified and carried out faster (no synchronisation necessary/programming, controlling) Vote Up +0 Vote Down -0You already voted!