At igus, we have the right sensors for linear systems, slewing ring bearings and plain bearings in the product range. They all belong to the products, which enable predictive maintenance. DLT.W – Sensor for wear in drylin T linear systems Is integrated in the liner Reports wear of the liner in good time This allows […]
Yes, that’s possible. The available communication interfaces make connecting to a higher-level industrial control system such as a PLC or an industrial PC very easy. But not only that … the D1 works just as well with microcontrollers like an Arduino or single-board computers like the Raspberry Pi. Thus, the D1 is also well prepared […]
A simple question but the only answers found are often technically complex. In simple terms, a linear guide is a means to move “something” from position A to position B in a straight line. This “something” can be a sliding door of a cabinet; it can be for a change of position or perspective of […]
What load do I want to move? How big is the thing that I want to move? What carriage surface is suitable for this? Is there a system in which I can choose between different widths and lengths? And what is the appropriate rail for this? What installation space is available to me? How can […]
The drylin N low-profile guide system consists of an anodised C-profile in which a sliding carriage travels. The basic carriage is a zinc die-cast component and is clipped into a sliding frame made of iglidur J polymer. Completely dry, clean and quiet when sliding. The two halves of the sliding frame can be ordered at […]