Motor control - igus Blog - Page 5 Motor control - igus Blog - Page 5

Category: Motor control

Can I also install the D3 DC motor control on a top-hat (DIN) rail?

Michael Hornung | 8. July 2019

Of course, if you want to install the D3 DC motor control compactly in a switch cabinet, that too works. This video shows how to implement a space-saving installation of a motor control on a top-hat DIN rail. Tip For those who want to know and read more about the operation of the D3 DC […]

Read more...

How do I install the D1 motor control in a switch cabinet?

Michael Hornung | 8. July 2019

The housing of the dryve D1 motor control allows a quick installation in a switch cabinet. The installation takes place vertically on a top-hat (DIN) rail and is therefore very space-saving. The bracket is standard on the housing. Just click and you’re done. You can see here how easy it is! Tip For those of […]

Read more...

How do I connect a mechanical proximity switch to a D3 DC motor control?

Michael Hornung | 8. July 2019

In addition to the inductive proximity switches, mechanical proximity switches can also be connected to the D3 DC motor control. You will find everything about the installation here. Tip For those who want to know and read more about the operation of the D3 DC motor controller, see here for the complete manual. Vote Up […]

Read more...

Which power supplies can be used with the D1 motor control?

Michael Hornung | 8. July 2019

The dryve D1 is THE motor control for stepper motors and DC motors. An explanatory video> will show you which power supplies can be used for the operation of the D1. The complete manual for the dryve D1 can be downloaded here. Vote Up +0 Vote Down -0You already voted!

Read more...

Is it possible to integrate the D1 into a higher-level control system?

Michael Hornung | 1. July 2019

Yes, that’s possible. The available communication interfaces make connecting to a higher-level industrial control system such as a PLC or an industrial PC very easy. But not only that … the D1 works just as well with microcontrollers like an Arduino or single-board computers like the Raspberry Pi. Thus, the D1 is also well prepared […]

Read more...