Cables/chainflex - igus Blog - Page 6 Cables/chainflex - igus Blog - Page 6

Category: Cables/chainflex

Why are cables wound in bundles?

Marco Thull | 8. July 2019

Cables with layered strands, 7 or more cores and a cross section of >1.0 mm² are especially at risk on long travels: The so-called corkscrew effect. This has an adverse effect on the cable’s overall structure and core breakages can occur. Cores wound in bundles counter this effect. Cable bundles with previously layered strands and […]

Read more...

What is important about a cable shield in moving applications?

Marco Thull | 8. July 2019

This depends on what kind of movement is involved. If torsional movement is involved, winding the shield around the stranding element is the most durable approach. In the case of movement in an energy chain, a very flat braiding angle is best because the braiding can open and close like a pair of scissors when […]

Read more...

What does CAT mean in the context of Ethernet cables?

Marco Thull | 8. July 2019

In order to describe the performance capability of a single component, the individual components of a network (cables and connectors) are categorised. In a network link, the component with the lowest performance capability (category) determines the transmission class of the entire system. Higher categories automatically cover the lower categories as well. The range is usually […]

Read more...

What is a measuring system cable?

Marco Thull | 8. July 2019

On servo drives, an encoder (encoder or resolver) is fitted for the precise determination of position. This electronic control signal must be taken to the drive control system in order to be evaluated there. So-called measuring system cables are used for this. These cables are to be made in accordance with the electrical stipulations of […]

Read more...

What is nominal voltage?

Marco Thull | 8. July 2019

The nominal voltage of an electrical load or a voltage source (battery, generator, power grid) is the electrical voltage during normal operation as specified by the manufacturer or supplier. Unless indicated otherwise, it is the RMS value of the voltage. Vote Up +0 Vote Down -5You already voted!

Read more...