Are there special energy chains with “Hygienic Design”?
Especially for the packaging, food and beverage industry special requirements are called for in the design of energy chains. These must be, for example, always easy to clean. The igus® energy chain series TH3 has been specially developed to meet these requirements. Their design is intended for efficient cleaning. In addition, there is no friction between the chain links, which minimises abrasion. If you need a hygienic design solution or a solution with FDA conformity, then contact us.


- All edges rounded
- Wide gaps (easy cleaning)
- No material on material wear (minimal abrasion)