Plain Bearings - igus Blog - Page 30 Plain Bearings - igus Blog - Page 30

Category:

Plain Bearings

Choosing plain bearing dimensions correctly – 3 tips

Lars Butenschön | 20. May 2020

Often enough, it is the surrounding factors such as housing hole, shaft and other elements that predetermine what plain bearing dimensions are chosen. Then whether a bearing with a length of 10mm or 12mm is selected only depends on the price or availability. But what about when these factors delimit the choice so tightly that […]

Read more...

igubal Metallgelenkkopf

Metal rod ends from igus, the plastics expert?

Peter Hughes | 18. May 2020

This month, igus® presented many new products in the framework of the virtual igus “KMI” trade show. One of the new igubal® products stands out especially: the new metal rod end. Is this a mistake in the New Products Catalogue? What does this product have to do with motion plastics? Much more than is apparent at first glance.

Read more...

Moulding of iglidur® plain bearings

Steffen Schack | 18. May 2020

Innovative developments in the automotive industry require intelligent production methods, especially in the case of component integration. One injection moulding method that has now become established is the so-called hybrid or 2C (two-component) technique. In this method, a component is placed in the injection moulding tool and moulded with a type of polymer. As a […]

Read more...

Exoskeleton – Bionics pure

Ulf Hottung | 15. May 2020

Widespread in the animal kingdom, for people an option. The skeleton on the outside of arthropods provides stability in the same way as the endoskeletons of mammals. Why not combine the advantages of the two systems with each other? An endoskeleton (inside the body) is strong but, having numerous joints, is nevertheless very flexible. It […]

Read more...

A (long) lifetime of the car without lubrication

Dirk Tietz | 13. May 2020

Many bearing positions in vehicles have to work without external lubricants such as grease or oil for their entire life, but must not fail or cause noise. How is this possible over many years? There are basically several types of lubrication: Consumption or loss of lubrication: old lubricant is continuously or cyclically replaced by new […]

Read more...