Plain Bearings - igus Blog - Page 28 Plain Bearings - igus Blog - Page 28

Category:

Plain Bearings

Coupling joints made of polymer – optimised materials for the automotive industry

Sebastian Bloechl | 8. June 2020

The coupling joint, also referred to as double joint, describes a strut with connection possibilities on both sides. Here, ball and socket joints, screw threads or sleeves can be inserted, which connect the coupling joint with the corresponding vehicle components. Usually, coupling joints are made of steel or aluminium. But for years, polymer coupling joints […]

Read more...

Save lubricant, prevent contamination & increase the service life of ball bearings

Patrick Czaja | 5. June 2020

Contaminated lubricant is one of the main causes of bearing damage and often a major factor in the premature end in the service life of bearings. Around 70% of bearing failures are caused by lubricant problems, such as contamination in the lubricant (25%), incorrect lubricant (20%) or too little lubricant (14%).

Read more...

Polymer bearings in adjustable seat posts

Alexander Muzicenko | 5. June 2020

The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]

Read more...

Polymer bearings in spring-mounted seat posts

Alexander Muzicenko | 5. June 2020

The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]

Read more...

Precise polymer bearing points in medical technology

Ulf Hottung | 5. June 2020

“Can’t be done!” say many design engineers and are therefore not generally wrong, but also not always right, especially in medical technology. Correct is: polymer bearings, or bearing points in polymer in general, are subject to various factors that influence the preferred bearing clearance. Impact on precision Correct is: polymer bearings, or bearing points in […]

Read more...