3D-Printing
Especially in times of crisis, creative and above all fast solutions are essential. And when it comes to speed and creativity, the 3D printing community is quick to respond. This was also the case this time when Prusa Research, a pioneer in FDM printing, created a design for 3D printed face shields and made it […]
Goods wagons are often in service for 30 years or even 40 years. Getting spare parts at the beginning is no problem. But what do you do if the supplier removes this component from his product range or the whole company shuts its doors? This is no problem with standard parts such as screws, seals […]
Every machine contains moving parts that cause friction during operation. In contrast to metal, components made of wear-resistant iglidur polymers do not require additional lubrication (because they contain solid lubricants) – however polymers cannot dissipate the electrostatic discharge caused by friction. In semiconductor and electrical engineering, a static discharge through components can cause permanent damage […]
3D printing is ascendant across industries and materials, not only in product development, but also in industrial manufacturing processes. But if the freedom granted by additive manufacturing is to realise its full potential in the industrial environment, 3D printing materials must perform just as well as their mechanically processed counterparts. igus has dedicated itself to […]
The two most common reasons for manufacturing drive and lead screw nuts using 3D printing processes are the construction of functional prototypes and the production of complex custom nuts. In product development, several models are sometimes designed and tested – with the rapid prototyping process, the production of near-series variants and customisations can be carried […]