Volker Beissel - igus Blog - Page 3 Volker Beissel - igus Blog - Page 3

Successful use of a 10m unsupported plastic chain

Volker Beissel | 2. April 2020

A gliding application frequently looks better than an unsupported energy chain. This is not just because the straight line of the upper run, but also because the sag leading to the chain drop is eliminated. This allows unsupported systems to better use the space at the end of the travel. But at high fill weights […]

Read more...

Strain relief on one or both sides?

Volker Beissel | 31. March 2020

It is known that strain relief can considerably increase the service life of cables and hoses in the energy chain. But an incorrect strain relief can also have the opposite effect. One point that comes up again and again is the question of whether strain relief should be mounted on one side or both sides? […]

Read more...

Can I also use the E4/4 rol e-chain in the machine tool?

Volker Beissel | 27. March 2020

The E4/4 rol e-chain is familiar from the crane industry among others. But what does this have to do with the machine tool? High loads, long travels and a dynamic behaviour, this description also frequently applies to x-axes in machine tools. The rol e-chain 5050RHD, for example, allows travels of 10-800m with a maximum fill […]

Read more...

What systems does igus offer for the machine tool’s X-axis?

Volker Beissel | 25. March 2020

In large machines, the X-axis is always a particularly great challenge. All supply lines the machine requires run through this e-chain, which can be very long. That is why reliability is especially important here. Because each machine tool is unique, we always try to find the best solution for the application in question.   The […]

Read more...