Lars Butenschön - igus Blog - Page 3 Lars Butenschön - igus Blog - Page 3

Locating spigot for bushings? This is how it works:

Lars Butenschön | 9. September 2022

There are many reasons for fixing bushings in the axial direction. If excessive forces act in the axial direction or external influences have a negative effect on the press-fit of the bearings, bushings are at risk of being pushed out of the bearing point. As a result, the shaft rotates in the housing hole “without […]

Read more...

Flanged bearing – what you need to think about

Lars Butenschön | 6. May 2022

In order to fix plain bearings in the receiving bore so that they are form-fitting, a collar or flange is attached on one side or, in some designs, both sides. If you use flanged bushings in your application, some design considerations will help avoid bearing damage. The housing hole The housing hole should be perpendicular […]

Read more...

Is gas nitrocarburising the best protection for bearing bolts?

Lars Butenschön | 1. April 2022

Corrosion protection of shafts and bearing bolts is especially critical if the bearing position is not to be lubricated. In more and more applications, lubrication of plain bearings is becoming a real problem (e.g. in the construction machinery industry). The frequently used galvanised shafts often turn out to be not resistant enough when used with […]

Read more...

Bolts and bearings for construction machinery under test: Hardox® and iglidur®

Lars Butenschön | 25. March 2022

The HARDOX® wearplates brand is frequently found in commercial vehicles and construction machinery where steel surfaces have to withstand the most severe stresses. From the loading area of tipper lorries to the bucket of wheel loaders, HARDOX® wearplates reliably protect against wear. For this reason, shafts and bolts made of HARDOX® are obvious counter partners […]

Read more...

Plain bearings – advantages and disadvantages at a glance

Lars Butenschön | 18. March 2022

You are faced with the decision to use a plain bearing, but you are not sure whether this is really the better choice compared to rolling bearings? Why not leave everything alone and simply do without a bearing? This post is intended to help you make that decision, in addition to providing a preview of […]

Read more...