All messages - igus Blog - Page 65 All messages - igus Blog - Page 65

How are plain bearings constructed?

Lars Butenschön | 4. March 2022

One of the main features of plain bearings – compared to ball or rolling bearings – is their significantly less complex design. But is that really the case? In fact, different types of plain bearings differ significantly in how they are constructed and how they work. In this blog post, you will learn all about […]

Read more...

Fast, fast, fast … Features of AG 5

Christian Strauch | 2. March 2022

An autoglide energy chain that does not require a guide trough has been available from igus for about 20 years. The principle of crossbars, which are designed like “tiewrap plates” so that the upper run can slide on the lower run while being fixed laterally, has been around for a long time. The decisive difference […]

Read more...

Gluing bushings – this is how it works

Lars Butenschön | 25. February 2022

Bushings are usually pressed or clamped into the housing hole. In this way they hold securely in the hole and do not rotate unintentionally. But what if this is not possible due to manufacturing tolerances? Another not so rare case: The bushing should even rotate. Even if it is not part of the standard repertoire […]

Read more...

A house from the 3D printer?

Christine Barreto | 25. February 2022

The design possibilities of 3D printing are endless. Civil engineers and architects take advantage of this. Most recently, a house in Beckum was 3D printed. Read more about the many uses of 3D printers in architecture in this article.

Read more...

Who wears shoes made of lead?

igu-blog-adm | 24. February 2022

The TV commercial for the Soda Streamer presents it perfectly. Who wants to carry anything heavy nowadays? One of the things using PET bottles as an alternative to glass bottles aims at is weight. The sustainability of the two solutions will be discussed at a later time. “The fact is that it takes energy to […]

Read more...