All messages - igus Blog - Page 224 All messages - igus Blog - Page 224

robolink News 2011

Martin Raak | 4. April 2011

robolink news and line extentions, more joints, connecting pipes and much more. Vote Up +0 Vote Down -0You already voted!

Read more...

Awarded design

Martin Raak | 1. December 2010

Robolink has been awarded by the “iF Forum Design GmbH” in the category “industrial design”. The iF awards are given particularly to innovative and visually appealing products. As one of the oldest competitions, the iF award is an internationally recognized design award. Award-winning igus® designs Vote Up +0 Vote Down -0You already voted!

Read more...

Angular sensor

Martin Raak | 1. June 2010

angular sensor Due to the integrated angular sensors, an arm can also be used directly as “teach-in” arm. Read-out angle information can be saved and called up or even directly transformed into movements (see film). Currently the sensor technology is advanced for series production. Development partner EvoLogics GmbH is a specialist for bionic inventions (the […]

Read more...

Hannover Messe

Martin Raak | 19. April 2010

The robolink highlights at the Hannover Messe 2010 – round tour through the stand and presentation of novelties. Vote Up +0 Vote Down -0You already voted!

Read more...

Development status

Martin Raak | 23. March 2010

Increase in the transmitted torque (rotation) from 5 (generation 1) to 7 Nm (generation 2) in continuous operation. (Damage in the one-off fracture test at > 24 Nm) GFRP and CFRP rods now available in profiled version. Maximum length of 1 m. See price list. Weight CFK: 170 g/m, GFK: 200 g/m, Aluminum 270 g/m […]

Read more...