The coupling joint, also referred to as double joint, describes a strut with connection possibilities on both sides. Here, ball and socket joints, screw threads or sleeves can be inserted, which connect the coupling joint with the corresponding vehicle components. Usually, coupling joints are made of steel or aluminium. But for years, polymer coupling joints […]
Goods wagons are often in service for 30 years or even 40 years. Getting spare parts at the beginning is no problem. But what do you do if the supplier removes this component from his product range or the whole company shuts its doors? This is no problem with standard parts such as screws, seals […]
“Can’t be done!” say many design engineers and are therefore not generally wrong, but also not always right, especially in medical technology. Correct is: polymer bearings, or bearing points in polymer in general, are subject to various factors that influence the preferred bearing clearance. Impact on precision Correct is: polymer bearings, or bearing points in […]
The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]
The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]