Is it possible to integrate the D1 into a higher-level control system? - igus Blog Is it possible to integrate the D1 into a higher-level control system? - igus Blog

Is it possible to integrate the D1 into a higher-level control system?

Michael Hornung | 1. July 2019

Is it possible to integrate the D1 into a higher-level control system?

You are here:

Yes, that’s possible. The available communication interfaces make connecting to a higher-level industrial control system such as a PLC or an industrial PC very easy.

But not only that … the D1 works just as well with microcontrollers like an Arduino or single-board computers like the Raspberry Pi. Thus, the D1 is also well prepared for IOT projects.

Here is a small list of control systems with which applications have already been implemented.

Depending on the customer’s requirements, digital inputs/outputs, cycle/direction signals, analogue inputs,

CANopen or Modbus TCP (gateway) were used as communication interface between D1 and higher-level control.

Siemens

  •                 Siematic Logo!
  •                 Siematic S7-1200
  •                 Siematic S7-1500
  •                 Siematic S7-300
  •                 Siematic S7-400

Servotronix

  •                 softMC301

Beckhoff

  •                 CX1020
  • CX5130

Mitsubishi

  •                 FX3G-40M

Raspberry Pi

  • Version 3
  •                 VersionVersion 2
  •                 Revolution PI

Arduino

  •                 Uno

BeagleBone

  •                 Black

Software for PC-based control systems

  •                 CODESYS
  •                 LabVIEW
  •                 MATLAB
You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Motor control

Newsletter:

Choose a topic now