How large can be the maximum cable diameter in the energy chain? - igus Blog How large can be the maximum cable diameter in the energy chain? - igus Blog

How large can be the maximum cable diameter in the energy chain?

Beke Nieszytka | 8. July 2019

How large can be the maximum cable diameter in the energy chain?

You are here:

To avoid abrasion of the cables, a clearance space between the cable and the chain is recommended. This is based on the inner height of the chain and the diameter of the cable.

Generally, the following formula applies:

  • Electrical cables: inner height -10%
  • Hydraulic hoses: inner height -20%
You already voted!
Tags:

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

cables

Newsletter:

Choose a topic now