What is the maximum temperature that the conductor can cope with according to DIN? (CU, CUZN, CUNI…) - igus Blog What is the maximum temperature that the conductor can cope with according to DIN? (CU, CUZN, CUNI…) - igus Blog

What is the maximum temperature that the conductor can cope with according to DIN? (CU, CUZN, CUNI…)

Marco Thull | 8. July 2019

What is the maximum temperature that the conductor can cope with according to DIN? (CU, CUZN, CUNI…)

You are here:

In principle, the temperatures occurring under load within a conductor differ according to what material is used. Pure copper has the best conductivity. However, the insulation used and the surface temperature affecting the insulation are also decisive for the maximum permissible temperature of a conductor.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Temperature

Newsletter:

Choose a topic now