Energy chain holding forces - igus Blog Energy chain holding forces - igus Blog

Energy chain holding forces

pwirth | 20. March 2020

How much force must I apply to open an energy chain?

The requirements of industrial applications are constantly increasing, and therefore the requirements for energy chain filling are too. The E4.80 series e-chains are usually used as soon as a substantial fill weight requirement arises.

This is important in milling linear robots in gantries, for instance. In the application examples listed below, three energy chain axes are installed. The X-axis is 10 metres long with a fill weight of 24kg/m. Among the elements it guides are hydraulic hoses with strong pulsation, which requires a great deal of energy chain holding force. The energy chain also travels with high acceleration (5m/s²).

A nice example of the forces necessary to open igus energy chains can be seen in the video below. Another application example with high holding force requirements can be found here

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!