It is not only nerves that are threatened by squeaking plain bearings. Squeaky bearings and bearings that make other noises can be a real noise pollution issue. For this reason, I will take a closer look at the topic of squeaking today. How it is generated and what can be done about it. This podcast […]
As a well-known manufacturer of engineering plastics, igus has meanwhile established itself in the minds of the engineering universe. But around these core products a huge product world has developed with over 10,000,XXX different products. One of them is the lead screw motor. As the name suggests, a lead screw motor consists of a lead […]
I don’t know any electrician who enjoys stripping cables. Stripping is no fun on a workbench. At a machine, the lack of space and poor lighting often presents us with completely different challenges and also involves a risk of injury. In a control cabinet between terminal blocks and other components, it is just not possible […]
There are probably few problems that are so annoying and so difficult to fix. Whether in a car, a bicycle or in the fully automated and fully digitalised industry 4.0 IoT packaging machine: disturbing noises. Squeaking plain bearings are of course only one possible source but more often than you think. Once the source has […]
Many metallic rolling bearings are available as a sealed version Ball bearing seals are usually mandatory for the metallic version, otherwise dirt will get into the running surfaces of the ball. They can combine with the lubricant and block the bearing run. Ball bearings made of polymer or ceramic are mostly only available as an open type. Why? Find out here.