May, 2020 - igus Blog - Page 7 May, 2020 - igus Blog - Page 7

Insert energy chain on the side

mkogelmann | 5. May 2020

The installation space for energy chains is often limited in height. One solution, although not always practical, is then to reduce the bend radius of the energy chain. But this is not always possible. Either the reduction of the bend radius is not sufficient for the chain to fit into the installation space, or it […]

Read more...

iglidur I8-ESD: abrasion-resistant components with ESD specifications

Paul Gomer | 5. May 2020

Every machine contains moving parts that cause friction during operation. In contrast to metal, components made of wear-resistant iglidur polymers do not require additional lubrication (because they contain solid lubricants) – however polymers cannot dissipate the electrostatic discharge caused by friction. In semiconductor and electrical engineering, a static discharge through components can cause permanent damage […]

Read more...

The maximum tensile strain of a cable?

Jan Arnoldy | 5. May 2020

The maximum tensile strain of a cable is particularly important where cables are used in hanging applications. Because there the cable must carry its own weight. This is the case in the lifting movement of a storage and retrieval unit (SRU). The maximum tensile force for cables The maximum tensile strain indicates up to which […]

Read more...

Versatile vending machines: when future demand is for snacks instead of masks

Andrej Schmidt | 4. May 2020

Diversity is increasing, and with it the flexibility of vending machines. Whoever wants to sell masks today and snacks tomorrow can do so without any problems.

Read more...

Why does igus offer so many different cable types of the same kind?

Nils Jäger | 4. May 2020

If one takes a look at the chainflex catalogue, one quickly realises that igus has many different cable types of the same kind in its range. In the section on control cables alone there are 19 different cable ranges. Why is that? The range of control cables includes cables with overall shield as well as […]

Read more...