In order for an assembly or component to be allowed for use in a modern rail vehicle in Europe, the components must be tested and evaluated according to EN45545. This is a very time-consuming, bureaucratic process. The exposed surface, the weight of the component, and many other points must be considered for selection. So where […]
Things can get hot when we move into bakery technology. This is a special challenge for bearings. It takes special bearings and bearing materials to handle the high ambient temperatures. Bearings are often used in applications where temperatures exceed 200°C. There are a wide range of applications in ovens and their immediate vicinity in the […]
Where are stainless steel linear modules used, and what advantages does stainless steel have over other materials such as aluminium?
The two most common reasons for manufacturing drive and lead screw nuts using 3D printing processes are the construction of functional prototypes and the production of complex custom nuts. In product development, several models are sometimes designed and tested – with the rapid prototyping process, the production of near-series variants and customisations can be carried […]
igus motion plastics – tribologically optimised high-performance polymers for moving applications – are the result of decades of research and development work. Each igus material, known under the iglidur brand name (https://www.igus.eu/iglidur), is thoroughly tested in our 3,800m² test laboratory. We have a huge material selection and are constantly adding new materials developed for various […]