The performance of a crane is directly dependent on its electrification system. With various power supply options available and a range of application requirements to take into consideration, making a choice of which type of system to implement can be difficult. It is crucial to consider the advantages and disadvantages of prospective energy supply systems, […]
Reliable and dynamic cable management is one of the greatest challenges in modern crane technology. Virtually all modes of crane applications are facing intensifying requirements regarding travel distances, speeds and precision.
autoglide 5: Scope of delivery The autoglide 5 is a brand new product from igus. It is unclear to what extent the chain is offered. But at the moment we are working on being able to offer the complete package. That means: The autoglide 5 as such: Energy chain type 2400.07.075.0 with autoglide crossbars on […]
What is so special about Profinet cables compared to “normal” data cables? Are there differences in the Profinet cables? Read it for yourself!
How do I ensure an abrasion-resistant energy supply system in a cleanroom? Many manufacturing processes, e.g. the production of printed circuit boards on linear systems for high-precision adjustments, take place in cleanrooms and require mandatory regulations according to ISO 14644 or VDI 2083. However, this alone does not guarantee absolutely clean production, as the materials […]