Why fibre optic cables? - igus Blog Why fibre optic cables? - igus Blog

Why fibre optic cables?

Max Herrmann | 9. July 2020

Most of us know the term fibre optic cable also under the name glass fibre cable. This topic is very much present among us because we know it from the media. Almost daily we are literally “connected” with it. Fibre optic cables have been providing fast and good Internet transmission for several years. Not only at home but also in industry.

We often have the picture of a small construction site with a large cable drum in our minds, where the fibre optic cable is being installed. Especially for long cable lengths, the fibre optic cables offer immense advantages over a copper conductor. Our customers often ask the situations where we recommend a fibre optic cable. You will learn the answer in the next few paragraphs.

What is a fibre optic cable?

A fibre optic cable – abbreviated as FOC – consists of fibres that can transmit light. The “conductor” consists of quartz glass or plastic. It transmits the light. For this purpose, electrical impulses are converted into a light pulse and transmitted via the cable by a light source. The light beam is reflected and transmitted within the fibres. As a result, it is also possible to transmit signals over a long distance. The fibre optic cable transmits the data using a light signal. Transmission of electrical energy is also possible, but is usually the exception.

Cable CFLG.G

Advantages over copper

Now we know what a fibre optic cable is, but what are the advantages over a copper conductor? Let us take a closer look at the four major advantages. Especially with long transmission lengths and data volumes, fibre optic cables clearly demonstrate their advantages over copper conductors.

Low signal attenuation and high transmission rates

In contrast to a copper conductor, the transmission of a fibre optic cable takes place with light and not with electric current. The optical transmission results in lower attenuation values. In contrast to copper conductors, these result in less signal loss over long distances. Higher frequencies and thus higher transmission rates can also be transmitted via the fibres of the fibre optic cable. This is also the reason why fibre optic cables are used in communications engineering and for our Internet connection.

Electromagnetic compatibility and mechanical specifications

Another great advantage of the fibre optic cable is its insensitivity to electromagnetic fields, the electromagnetic compatibility. While the signal in a copper conductor can be strongly influenced by external electromagnetic influences, the fibre optic cable is completely insensitive. This is due to the fibres of the fibre optic cable. No electric current can flow through or be induced in the fibres. The fibre optic cables can easily be laid directly next to other cables.

As a fourth advantage, igus has developed good mechanical specifications for small bend radii and long distances through intensive research. These specifications of the cable qualify chainflex for movement in the energy chain up to 5xd. Depending on the cable family, the fibre optic cables also have torsional resistance and are suitable for special climatic conditions or, of course, for long travels.

Application areas for chainflex fibre optic cables

Now we still have the image of the fibre optic cables under street level for an Internet connection in our minds. But where are our chainflex fibre optic cables used?  Right. Wherever fibre optic cables have their advantages over copper conductors. These include production lines or cranes where signals must be transmitted over long distances. Industrial bus systems in particular quickly reach their limits when transmitting over long distances with a copper conductor. In contrast, the transmission of the bus signal via the fibre optic cable is smooth.

We offer a variety of fibre optic cables with special jackets made of PVC, PUR or TPE. In addition, our cables have a perfectly matched structure with guaranteed service life in energy chain applications. Be it for special media resistance, high accelerations and speeds or simply resistance to oils and coolants.

Conclusion

Our chainflex fibre optic cables can be found in the most diverse areas. The four advantages: low signal attenuation, high transmission rates, good electromagnetic compatibility and the special mechanical specifications. These specifications lead to the choice of a fibre optic cable not only in communications engineering but also in industry. It provides reliable transmission for sensitive data and signals.

Are you wondering whether a fibre optic cable is the right choice for your application? We would be pleased to advise you on the selection of the right cable for your application. We are happy to offer you the cable as a ready-made system. Please contact us!

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!