Seal
Many metallic rolling bearings are available as a sealed version Ball bearing seals are usually mandatory for the metallic version, otherwise dirt will get into the running surfaces of the ball. They can combine with the lubricant and block the bearing run. Ball bearings made of polymer or ceramic are mostly only available as an open type. Why? Find out here.
Everyone knows that the agricultural and construction machinery sector require lots of care. Dirt, moisture, corrosion, the complete package. Whether a combine harvester, tractor, concrete mixer, plough or mobile crane – here everything is in the same boat. Metallic plain bearings are always lubricated – at least they should be if they are to function. […]
Many metallic rolling bearings are available as a sealed version The sealing is usually absolutely necessary for metallic ball bearings as otherwise dirt can get into the ball running surfaces, mix with the lubricant and thus block the rolling of the bearing. Metallic bearings must be protected Metallic ball bearings are also available in an […]