Plastic ball bearings - igus Blog - Page 4 Plastic ball bearings - igus Blog - Page 4

Keyword:

Plastic ball bearings

xiros guide rollers with FDA conformity: 60% weight saving compared to metallic solutions

Patrick Czaja | 10. July 2020

This solution for transport and guide rollers is now available in a lighter, FDA-compliant version. The xiros guide rollers for labelling, packaging and food applications consist of a blue PVC tube and two fixed flange ball bearings made of the in-house material xirodur B180 and stainless steel balls. The specialist for plastics in motion, igus, […]

Read more...

Why lubrication-free is a better option for your ball bearing

Patrick Czaja | 15. June 2020

Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines! In most applications where ball bearings are used, mainly low loads and low speeds are required. Plastic ball bearings can be used in multi-functional applications, for example, in cases where they come into contact with liquid media, water or chemicals.

Read more...

Save lubricant, prevent contamination & increase the service life of ball bearings

Patrick Czaja | 5. June 2020

Contaminated lubricant is one of the main causes of bearing damage and often a major factor in the premature end in the service life of bearings. Around 70% of bearing failures are caused by lubricant problems, such as contamination in the lubricant (25%), incorrect lubricant (20%) or too little lubricant (14%).

Read more...

Where metal ball bearings reach their limits: an opportunity for the polymer version?

Patrick Czaja | 6. May 2020

Metal ball bearings have become indispensable in mechanical and plant engineering. However, there are sectors where conventional metal ball bearings reach their limits, such as the food industry and medical technology. There the factor of hygiene plays a major role, which makes lubricants a no-go.

Read more...

Vehicle interior – 3 examples of polymer ball bearings in control elements

Sebastian Bloechl | 23. April 2020

The modern car interior has many different knobs, dials and switches. Whether it is the adjustment of the window, air conditioning or sound level – we are increasingly resorting to the cleverly placed rotary adjusters in the interior. All these controls are directly related to the quality perception of the vehicle and can influence a possible car purchase.

Read more...