Motor cable drum
Guide cables and hoses safely in limited installation space without rapid fatigue fractures that lead to expensive downtime: an ultimate discipline! The possibilities offered by compact energy chains and highly flexible cables. Building a house in the country, on a 1,000m2 plot: no problem. It gets trickier in a 200m2 small gap in a big […]
The lift band was specially developed for vertical applications on indoor / EOT cranes. A spiral energy chain that can be stored in a collecting basket. The cables are routed through the spiral energy chain without being exposed to any tensile stress. The retainer belts attached to the system ensure that the energy chain is safely stored in the special basket. The system is light, requires very little space on the lifting device and it is almost maintenance-free.
The e-spool is a chain-based drum application without sliding contacts. Ideal for applications and load-carrying equipment constructions that have no room for a collection basket (lift strap). The cables guided in the chain are not exposed to tensile strain, which has a positive effect on the service life of the cables.
liftband was specifically developed for vertical applications on indoor cranes. A spiral-shaped energy chain that can be placed in a collection basket. The cables are guided in the spiral-shaped energy chain without any tensile strain. The straps attached to the system ensure that the energy chain remains safe in the collection basket. The system is light, requires very little installation space on the load suspension device and is virtually maintenance-free.
Generic terms The term e-chain is closely related to the terms drag chain, energy chain and energy supply system or energy guiding chain or even cable guidance systems. The e-chain describes a product which safely carries cables or even hoses, over a certain distance. They ensure the dependable supply of energy, data and signals while […]