Metal bearing
Bronze bushings, like many other purely metallic bushings, are based on a so-called alloy. In this process, metallic “mixtures” are created by melting together different types of metal, which in turn have different specifications. A direct comparison of these different alloys with the no less numerous different polymer compounds, which are common in polymer bearings, […]
Within the industry, plasma technology has established itself as a technical standard for optimising material surfaces. Atmospheric pressure plasmas are created, for example, by electrical discharges in the air or by other gases. They enable remarkable material surface treatment due to a large amount of reactive and short-lived chemical species. The species clean, disinfect and […]
Whether at the largest manufacturer of rubber gloves in Malaysia or at a specialist in the packaging process of condoms in Thailand: machines in latex processing depend on durable and fail-safe components to avoid downtime. Metal ball bearings are used in a wide range of applications. However, the deployment could turn out to be a […]
Spring is approaching, the weather is getting better and the hours of sunshine are increasing again. Especially in summer, when heat is an added factor, sun shades play an important role. The reliable shading of a room not only ensures a pleasant working atmosphere, for example when working on a home computer, but also an […]