lubrication free
Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines! In most applications where ball bearings are used, mainly low loads and low speeds are required. Plastic ball bearings can be used in multi-functional applications, for example, in cases where they come into contact with liquid media, water or chemicals.
Many bearing positions in vehicles have to work without external lubricants such as grease or oil for their entire life, but must not fail or cause noise. How is this possible over many years? There are basically several types of lubrication: Consumption or loss of lubrication: old lubricant is continuously or cyclically replaced by new […]
Motorists with disabilities benefit from “Darios”, a digital gas ring. This allows you to give throttle with your hands on the steering wheel. “Darios 211” consists of over 200 identical parts that slide over the flattened steel ring. These parts consist of iglidur® I3 and are manufactured in 3D printing. How does the gas ring […]