liftband
liftband was specifically developed for vertical applications on indoor cranes. A spiral-shaped energy chain that can be placed in a collection basket. The cables are guided in the spiral-shaped energy chain without any tensile strain. The straps attached to the system ensure that the energy chain remains safe in the collection basket. The system is light, requires very little installation space on the load suspension device and is virtually maintenance-free.