e-chains®
The installation space for energy chains is often limited in height. One solution, although not always practical, is then to reduce the bend radius of the energy chain. But this is not always possible. Either the reduction of the bend radius is not sufficient for the chain to fit into the installation space, or it […]
Especially in machine tools, many electrical cables and hoses run through the energy chain. Hoses for hydraulics and cooling with large diameters are often necessary to meet the requirements of flow rates. This means that designers must select energy chains with a large interior space.
Installation situation e-chain with moving lower run Sometimes the installation situation requires turning the orientation of the e-chain and turning it upside down, so to speak. The fixed end is mounted “up” and the moving end is “down”. This is a very special installation situation and places other demands on the design of the energy […]
For historical reasons, energy chains have so far always been manufactured from steel or plastic. Steel has the advantage of allowing longer unsupported lengths. A plastic energy chain has various advantages, including lower cost and faster installation. There is now a new product: the hybrid steel-plastic chain. The energy chain is built with steel inner […]
Generic terms The term e-chain is closely related to the terms drag chain, energy chain and energy supply system or energy guiding chain or even cable guidance systems. The e-chain describes a product which safely carries cables or even hoses, over a certain distance. They ensure the dependable supply of energy, data and signals while […]