cables - igus Blog - Page 12 cables - igus Blog - Page 12

Keyword:

cables

The difference between a servo cable and a motor cable

Nils Jäger | 25. March 2020

Electrical engineering is often concerned with motor cables as well as servo cables. But what is exactly the difference between a servo cable and a motor cable? And can I use a servo cable to connect a normal three-phase motor? What exactly are the differences? The fact is that both cables are designed to supply […]

Read more...

Medikamenten-Handling in der Apotheke

What requirements do energy chains encounter in automatic medication handling applications?

Beke Nieszytka | 25. March 2020

Harnessed energy chains in automatic medication picking systems face special requirements.

Read more...

Why are there Ethernet cables with 600V UL?

Jan Arnoldy | 24. March 2020

Before we turn to Ethernet cables with 600V UL, let’s take a look at Ethernet cables generally. Ethernet is the most widely used standard for local area network (LAN) cabling. Although transmission rates of up to 400 Gbps are currently specified, a maximum speed of 40 Gbps is possible according to the current state of […]

Read more...

CF Profinet

Profinet cables – Why?

igu-blog-adm | 18. March 2020

What is so special about Profinet cables compared to “normal” data cables? Are there differences in the Profinet cables? Read it for yourself!

Read more...

Identify cables in the medical device

Ulf Hottung | 11. February 2020

Just a small detail and hopefully never important… The traceability of igus chainflex cables. Just a small detail and hopefully never important… The traceability of igus chainflex cables. EVERY igus chainflex cable is provided with a code on its jacket as in the following picture, which shows the manufacturing plant AND batch, the production date […]

Read more...