Bearing technology
Wear results of our new material iglidur® K250, which is characterised by a high flexibility and moisture absorption, are presented below. Compared to the igus classic iglidur® M250, the tribological properties could also be improved.
Maximum vehicle efficiency requires harmonised thermal management. Optimum operating temperature ensures efficiency and thus the lowest consumption and associated emissions. Coolant plays an important role – it cools, provides corrosion protection and prevents frost. Coolant pumps, regulators and valves distribute coolant throughout the vehicle, sending it where it is needed. Find out more here. In […]
Cosy heating in the winter and an air-conditioned living room in the summer – in addition to such everyday concerns, thermal management plays a decisive role in the automotive industry. In that industry, for instance, it is the engine that meets various scenarios. At first, it needs a temperature rise that is as quick as […]
There are a large number of standards in the railway industry. How much force is required to open a door by hand in an emergency? How should the welding seams look? The number of standards and regulations is seemingly endless. Another very important point is fire protection in rail vehicles. The EN 45545 standard means […]