Servo cable for motors in high frequency control - igus Blog Servo cable for motors in high frequency control - igus Blog

Servo cable for motors in high frequency control

igu-blog-adm | 2. July 2019

CF27.D with folded shield pair for easy processing

Today’s high-frequency-controlled drives and motors, so-called Variable Frequency Drives (VFD), are demanding and technically sensitive. The servo cables used for this purpose are therefore not only means to an end, but ultimately even tip the scale. Why? Because even the nature of the materials used, in this case, the insulation material, can have a huge impact on the entire drive. Therefore we at igus® have optimised the servo cables for the motors that are operated on a VFD or even a converter.

Frequency converters need suitable equipment

Our claim as a specialist for cables in energy chains rests upon our ability to always develop the optimum component for the respective field of application and to respond to current market developments with new insulation materials. The starting point for our igus® developers was as follows: The capacitance values of the cables are having an increasing effect in the compact frequency converters because the signal edges are becoming steeper and steeper. At the same time, the compensation must be increasingly compact for reasons of space. So we asked ourselves: Which cable insulation can lead to a lower energy loss than with the classic PVC insulation in motors with high-frequency control?

New insulation as a way to efficiency

Thanks to our decades of experience in the development of high-performance polymer materials, we have found the solution right here. Our chainflex® servo cables for energy chains are produced with a low capacitance (low dielectric constant) insulation material made of a special high-performance polymer. They show optimal test results and have also proven themselves in practical tests. For the customers, this means that they do not run the risk of encountering the electrical limits of the converter system and thus can utilise the latest technology of the most diverse drive manufacturers.

A service that is a matter of course for us is that we harness the cables with the appropriate connectors specified by the drive. And that from one piece in any length and jacket quality. Of course, our proven 36-month guarantee also applies to all chainflex® servo cables.

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!