…mm (drill hole diameter of the sleeves = 2 mm, outer diameter of the needle = 1 mm).
https://www.youtube.com/user/RoboticsEurope
Vote Up +0 Vote Down -0You already voted!…
…and long service life. xiros slewing ring ball bearings fill this profile requirement perfectly, and one reason is that customer-specific requests can be implemented without any problem.
https://www.youtube.com/watch?v=VWQ3Bg_8q_I
Are…
…manufacturing process Complex models can be created Just-in-time production Lightweight solutions easy to implement Fast alterations and adaptations possible Easy manufacture of filigree models No tool or set-up costs https://www.youtube.com/watch?v=ceXU-bgv-74 HEXAGON…
…and is also referred to as the fused layer modeling method. The plastic or metal material that is processed is called filament.
The filament must reach a liquid state…
…a WINDOWS software package.
https://www.youtube.com/watch?v=8fojZpPTgJE&feature=youtu.be
More details can not yet be announced, as this is a brand new solution, but we will check more facts within the next…