…4. Furthermore, a plastic bearing offers a weight saving of up to 80% compared to metallic bearings. Especially in cycling, the weight of the bike plays an important role –…
The temperatures are slowly rising, spring is approaching and the bike is ready. Various bike tours through the country, mountain biking through mountainous terrain or a tour through the
…
…polymer bearings in this demanding application are shown below.
High speeds are reached during rapid off-road descents and it is therefore important to maintain control of the bike in…
Crankbrothers bicycle pedals with iglidur plain bearings (source: igus GmbH)
The bicycle is still very popular as a means of transportation. But whether the bike in question is a
…
…must not cause the doors to sag, which would negatively influence the externally visible gap dimensions.
Where plain bearings are used: mountain bikes Mountain bike with plain bearings (Source: igus…