Water absorption - igus Blog Water absorption - igus Blog

Tag: Water absorption

What is the difference between “maximum moisture absorption” and “maximum water absorption” on the material data sheet?

Lars Butenschön | 9. July 2019

The test of “maximum moisture absorption (at 23° C/73° F, 50 % r.  h.)” is a testing method according to DIN 53495 and provides information on the amount (namely the increase in volume of the component)l of moisture absorbed from the air. The information in brackets describes the air temperature and humidity, whereas “maximum water absorption” means the […]

Read more...