USB cable - igus Blog USB cable - igus Blog

Tag: USB cable

Up to what length do USB cables function?

Marco Thull | 8. July 2019

The maximum possible length of USB cables varies considerably and is defined in the bus specification for USB. The maximum lengths are different and depend on whether USB 2.0 or USB 3.0 is concerned. For USB 2.0, the maximum cable length is approximately 5m, for USB3.0 approximately 3m. But the cable length can vary from […]

Read more...