Motor control - igus Blog - Page 3 Motor control - igus Blog - Page 3

Tag: Motor control

Which power supplies can be used with the D1 motor control?

Michael Hornung | 8. July 2019

The dryve D1 is THE motor control for stepper motors and DC motors. An explanatory video> will show you which power supplies can be used for the operation of the D1. The complete manual for the dryve D1 can be downloaded here. Vote Up +0 Vote Down -0You already voted!

Read more...

Can I set different acceleration profiles in the D3 DC motor control?

Michael Hornung | 8. July 2019

That works. And yes, right on the housing. And yes it’s really easy. Because, the D3 DC motor control offers a selection between 5 different acceleration settings (also acceleration profiles or ramps).  And the selection is carried out like this. Tip For those who want to know and read more about the operation of the […]

Read more...

How do I know the IP address of a D1 motor control?

Michael Hornung | 8. July 2019

A hallmark of a modern motor control system for stepper and DC motors is the ease of use. But before the simple operation is the easy connection. And that’s especially easy with the dryve D1 motor control. Without any software just enter the IP of the D1 in the browser of your choice and off […]

Read more...

What all can I adjust directly on the D3 DC motor control?

Michael Hornung | 8. July 2019

You do not need a laptop, pad or smart phone to operate the dryve D3 DC motor control. The most important functions can be found directly on the housing and this makes the motor control very mobile and very easy to operate. Convince yourself. Vote Up +0 Vote Down -1You already voted!

Read more...

Do not take it too seriously. The D3 DC motor control in alternative use.

Michael Hornung | 8. July 2019

Even unusual applications can be implemented with the D3 DC motor control. Everything is possible, because the operation is very simple. The control system on the housing itself enables mobile use. You can see a few ideas here. … and you can buy the DC motor control here. No minimum quantity, and delivered in 24 […]

Read more...