Linear plain bearing - igus Blog Linear plain bearing - igus Blog

Tag: Linear plain bearing

The assembly advantage of a split linear plain bearing

Michael Hornung | 5. July 2019

As an alternative to lubricated ball bushings, there is the clean self-lubricating alternative of a linear plain bearing adapter. The two cylindrical types have identical installation heights and can be installed in any linear housing. The assembly in the housing is also identical for both bearings. With a split housing, the replacement of the bearing […]

Read more...

How is a linear plain bearing installed?

Michael Hornung | 30. June 2019

As an alternative to lubricated ball bushings, there is the clean, self-lubricating linear bearing adapter. The two cylindrical types have identical installation heights and can be installed in any linear housing. The two bearing types are also installed in the housing in exactly the same way. Firstly, a circlip is inserted into the inner groove […]

Read more...