KMA - igus Blog KMA - igus Blog

Tag: KMA

Why is an angled moving end bracket beneficial?

Phillip Hagedorn | 3. July 2019

With a mounting angle between 3-5°, the e-chain is slightly forced downward by the push/pull force. This prevents the rising up of the e-chain. The angle of incidence of the upper run to the lower run is approximately 3-5°. This angle is also ideal for reducing wear. If the upper run is installed in parallel […]

Read more...