Extension link - igus Blog Extension link - igus Blog

Tag: Extension link

What is an extension link and what does it do?

Phillip Hagedorn | 3. July 2019

The extension link is an additional link, which is connected to the two outer bands by means of crossbars. The extension link increases the possible load capacity (+50% per extension link) of an E4 energy chain series and also allows widths of up to 3,000 mm.  For more information, please contact us! Vote Up +0 […]

Read more...